Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24783
  • Release Date : 2019/02/27 16:16
  • Print

Data backup failure

Although the latch (backup) area is set, the data is not latched.
Category : 

Answer

If the OUT instruction using the device number of the latch target device exists in a sequence program, the latched data may be overwritten by execution of the OUT instruction.
Use the SET instruction instead of the OUT instruction for the device numbers that need to be latched.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main unit, Engineering Software, GX Works2, GX Developer
Series
MELSEC-F series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?