Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24785
  • Release Date : 2019/02/27 16:31
  • Print

Distinguishing the usage of standard counters and high-speed counters

How can I distinguish the usage of standard counters and high-speed counters?
Category : 

Answer

Standard counters offer counting up to 10Hz.
For high-speed input signals which exceed 10Hz, use high-speed counters, interruption function, or another processing method which is not affected by the input filter and operation the cycle of a programmable controller.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main unit, Engineering Software, GX Works2, GX Developer
Series
MELSEC-F series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?