Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24787
  • Release Date : 2019/02/28 09:06
  • Print

Counting of a built-in high-speed counter

When a built-in high-speed counter does not start counting, what are the possible causes?
Category : 

Answer

Check that the RST instruction of the high-speed counter is not executed while the program is running.
For the high-speed counter which supports the external reset input, check that the external reset input is not on.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main unit, Engineering Software, GX Works2, GX Developer
Series
MELSEC-F series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?