Start main contents
Font Size
S
M
L
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Counting of a built-in high-speed cou...
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
No : 24787
Release Date : 2019/02/28 09:06
Print
Counting of a built-in high-speed counter
When a built-in high-speed counter does not start counting, what are the possible causes?
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
Check that the RST instruction of the high-speed counter is not executed while the program is running.
For the high-speed counter which supports the external reset input, check that the external reset input is not on.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main unit, Engineering Software, GX Works2, GX Developer
Series
MELSEC-F series
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
Models of the MELSEC-F series main units
Writing a program to a memory cassette
Assignment of remote input device and...
Ethernet-connectable modules in MELSEC-F
Externally switching the operating st...
page top
HOME
FAQ