Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24868
  • Release Date : 2019/04/15 08:06
  • Print

Assignment of input/output numbers (MELSEC-F series)

Answer

Octal numbers are assigned as input/output numbers for the MELSEC-F series.
The octal number system uses the digits from 0 to 7 → from 10 to 17 → from 20 to 27・・・from 70 to 77 → from 100 to 107.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main Unit, Engineering Software, GX Works2, GX Developer
Series
MELSEC-F Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?