Start main contents
Font Size
S
M
L
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Assignment of input/output numbers (M...
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
No : 24868
Release Date : 2019/04/15 08:06
Print
Assignment of input/output numbers (MELSEC-F series)
How are the input/output numbers assigned? (MELSEC-F series)
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
Octal numbers are assigned as input/output numbers for the MELSEC-F series.
The octal number system uses the digits from 0 to 7 → from 10 to 17 → from 20 to 27・・・from 70 to 77 → from 100 to 107.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main Unit, Engineering Software, GX Works2, GX Developer
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
Changing the time of a programmable c...
Power supply cable of the input exten...
No communication between a programmab...
Counting of a built-in high-speed cou...
How to use built-in high-speed counters
page top
HOME
FAQ