Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24876
  • Release Date : 2019/04/15 08:07
  • Print

No communication between a programmable controller and a personal computer (GX Developer) after the communication parameters for the RS-232C communication equipment are set

A programmable controller became unable to communicate with GX Developer after the communication parameters for the RS-232 communication equipment are set.
Category : 

Answer

To establish communications between the programmable controller and GX Developer, clear the communication setting. (The communication setting register value must be 0.) On GX Developer, uncheck the "Operate communication setting" checkbox in the "PLC system(2)" tab of PLC parameter.
Product Name
FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main Unit, Engineering Software, GX Developer, GX Works
Series
MELSEC-F Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?