Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24906
  • Release Date : 2019/04/15 11:32
  • Print

Using an expansion board and a special adapter together

Is it possible to use a built-in expansion board of a programmable controller and an external special adapter together?
Category : 

Answer

In the FX1S/FX1N/FX2N series, only the expansion board for special adapter connection can be used together with the special adapter.
In the FX3G series (only 40/60-point types), FX3U series, and FX3UC series (only -LT/-LT2 types), the extension board for communications and the special adapter can be used together.
Product Name
MELSEC-F Series
Product Category
FX3G, FX3U, FX3UC
Series
Main Unit, I/O Extension
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?