Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24911
  • Release Date : 2019/04/15 11:32
  • Print

Power supply cable of the input extension blocks for the connector type programmable controllers

What is the model and connection method of the power supply cable of the input extension blocks for the connector type programmable controllers?
Category : 

Answer

For the first input extension block connecting to a main unit, use the FX2NC-100BPCB power supply cable provided with the main unit, and supply power from a 24 V DC power supply. For the second or later input block, use the FX2NC-10BPCB1 power supply cable provided with the input extension block, and connect it to either upper or lower power supply connector of the input extension block previously connected.
Product Name
MELSEC-F
Product Category
FX1NC, FX3GC, FX2NC, FX3UC
Series
Main Unit, I/O Extension
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?