FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Differences in the specifications between the programmable controllers used in Japan and overseas.
FAQ
Differences in the specifications between the programmable controllers used in Japan and overseas.
What are the differences between the programmable controllers used in Japan and overseas?
- Category :
Answer
The input signal forms are different. All the programmable controllers for the domestic market other than the FX3G/FX3U series are the sink input. The programmable controllers for the overseas market and the FX3G/FX3U series can switch the sink/source input. Also, transistor outputs differ between the sink output type and source output type.
All the products of the FX3G/FX3U series are compliant with the overseas standards.
For the models other than the FX3G/FX3U series, the products for the overseas market are compliant with overseas standards.
All the products of the FX3G/FX3U series are compliant with the overseas standards.
For the models other than the FX3G/FX3U series, the products for the overseas market are compliant with overseas standards.
- Product Name
- MELSEC-F Series
- Product Category
- FX1S, FX1N, FX1NC, FX3G, FX3GC,FX2N, FX2NC, FX3U, FX3UC
- Series
- Main Unit