FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Supported versions of the FX3U/FX3UC series main units for the CC-Link parameter settings using GX Works2
FAQ
Supported versions of the FX3U/FX3UC series main units for the CC-Link parameter settings using GX Works2
Which versions of the FX3U/FX3UC series main units support the CC-Link parameter settings using GX Works2?
- Category :
Answer
Ver.3.10 or later is applicable. (GX Works2 with Ver.1.73B or later is applicable.) The version of the main unit can be checked with the last three digits of the data stored in the special register D8001 (PLC type and system version).
(Example) When the special register D8001 is monitored using GX Works2 and the numerical value stored in the D8001 is a decimal number "24310", the last three digits "310" represent the version.
(Example) When the special register D8001 is monitored using GX Works2 and the numerical value stored in the D8001 is a decimal number "24310", the last three digits "310" represent the version.
- Product Name
- MELSEC-F Series
- Product Category
- FX3U,FX3UC
- Series
- Main Unit