Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24920
  • Release Date : 2019/04/17 11:41
  • Print

Maximum number of personal computers that can be communicated with the FX3U-ENET-L simultaneously

How many personal computers can be communicated with the FX3U-ENET-L simultaneously?
Category : 

Answer

For communications using MELSOFT connection, such as GX Developer, GX Works2, GOT1000, and MX Component, up to two personal computers can be used.
In addition, up to two lines can be connected in combination of sending or receiving data in the fixed buffer (non-protocol) communication.
Product Name
MELSEC-F Series
Product Category
FX3U, FX3UC
Series
Network/Communication
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?