FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Network/Communication > Maximum number of personal computers that can be communicated with the FX3U-ENET-L simultaneously
FAQ
Maximum number of personal computers that can be communicated with the FX3U-ENET-L simultaneously
How many personal computers can be communicated with the FX3U-ENET-L simultaneously?
Answer
For communications using MELSOFT connection, such as GX Developer, GX Works2, GOT1000, and MX Component, up to two personal computers can be used.
In addition, up to two lines can be connected in combination of sending or receiving data in the fixed buffer (non-protocol) communication.
In addition, up to two lines can be connected in combination of sending or receiving data in the fixed buffer (non-protocol) communication.
- Product Name
- MELSEC-F Series
- Product Category
- FX3U, FX3UC
- Series
- Network/Communication