Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24926
  • Release Date : 2019/04/17 11:42
  • Print

Adding two channels of the RS-232C port in the FX3G series

I would like to add two channels of the RS-232C port in the FX3G series. How can I add the communication expansion boards and adapters?
Category : 

Answer

Select the 40-point or 60-point type FX3G series main unit. In this case, two FX3G-232-BDs can be connected. When  FX3G-CNV-ADP is used, an FX3U-232ADP can be used instead of an FX3G-232-BD.
Product Name
MELSEC-F Series
Product Category
FX3G
Series
Main Unit
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?