Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24929
  • Release Date : 2019/04/17 11:42
  • Print

Communication format setting

Answer

The communication format can be set in the communication setting of a sequence program or "PLC Parameter setting" using GX Developer.
To avoid setting troubles, use either method.
Product Name
MELSEC-F Series
Product Category
FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Series
Main Unit, Engineering Software, GX Works2, GX Developer
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?