FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Overwriting a current value with the high-speed counter comparison instruction
FAQ
Overwriting a current value with the high-speed counter comparison instruction
The output contact is not set by overwriting the current value with the MOV instruction while using the high-speed counter comparison.
- Category :
Answer
The output contact is activated according to the change of the current value register along with the counting input. Therefore, the value changed by executing the MOV instruction is not set before the next count input is received.
- Product Name
- MELSEC-F
- Product Category
- FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Series
- Main Unit
May I have your opinion?
Related FAQ
- Maximum number of personal computers that can be communicated with the FX3U-ENET-L simultaneously
- Index modifier of bit devices in the FX3G series
- Drive products (servo amplifiers) that can be connected to the FX3U-1PG pulse output block
- Using a fixed latched (battery backed) type device as a general type device
- Supported versions of the FX3G/FX3GC series main units for the CC-Link parameter settings of GX Works2