FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Number of FX3U-ENET-ADP Ethernet communication special adapters that can be connected to the FX3UC series
FAQ
Number of FX3U-ENET-ADP Ethernet communication special adapters that can be connected to the FX3UC series
How many FX3U-ENET-ADPs can be connected to the FX3UC series?
- Category :
Answer
One FX3U-ENET-ADP can be connected at the last stage (left end) of adapters for the FX3UC series.
*The FX3U-ENET-ADP is a communication special adapter and occupies one communication channel.
・ When the FX3U-ENET-ADP is used with the FX3UC-32MT-LT (-2) programmable controller, another expansion board/communication special adapter (including the FX3U-8AV-BD/FX3U-CF-ADP) can be used.
・ When the FX3U-ENET-ADP is used with the FX3UC (D/DS/DSS) programmable controller, another communication special adapter (including the FX3U-CF-ADP) can be used.
*The FX3U-ENET-ADP is a communication special adapter and occupies one communication channel.
・ When the FX3U-ENET-ADP is used with the FX3UC-32MT-LT (-2) programmable controller, another expansion board/communication special adapter (including the FX3U-8AV-BD/FX3U-CF-ADP) can be used.
・ When the FX3U-ENET-ADP is used with the FX3UC (D/DS/DSS) programmable controller, another communication special adapter (including the FX3U-CF-ADP) can be used.
- Product Name
- MELSEC-F Series
- Product Category
- FX3UC
- Series
- Main Unit