Start main contents
Font Size
S
M
L
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Connecting special adapters to FX3U s...
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
No : 24934
Release Date : 2019/04/18 14:23
Print
Connecting special adapters to FX3U series
Are any interface modules required for connecting special adapters to FX3U series?
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
I/O Extension
Answer
An expansion board is required. (However, it is not required when connecting only the special high-speed I/O adapter.)
Product Name
MELSEC-F Series
Product Category
FX3U
Series
Main Unit, I/O Extension
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
Cable provided with the FX2N series e...
24+ terminal connection of an extensi...
Power supply cable of the input exten...
CF cards that can be used in the FX3U...
Extension blocks and units that can b...
page top
HOME
FAQ