Start main contents
Font Size
S
M
L
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Main Unit
>
Extension blocks and units that can b...
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
No : 24935
Release Date : 2019/04/18 14:24
Print
Extension blocks and units that can be used in the FX3U series
Is it possible to use the FX0N series extension blocks and units with the FX3U series?
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
I/O Extension
Answer
The operation is not guaranteed. Please select the extension blocks and units from FX2N series.
Product Name
MELSEC-F Series
Product Category
FX3U
Series
Main Unit, I/O Extension
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
Connecting special adapters to FX3U s...
Number of FX3U-ENET-ADP Ethernet comm...
Cable provided with the FX2N series e...
Number of files that can be created i...
24+ terminal connection of an extensi...
page top
HOME
FAQ