Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24941
  • Release Date : 2019/04/18 14:25
  • Print

Extending the extension cable

Is it possible to extend the length of the extension cable to over 65 cm?
Category : 

Answer

It is not possible to extend the length of the extension cable to over 65cm. Place the main unit separately by using the parallel link or N:N Network function or configure a distributed system by using CC-Link or CC-Link/LT.
Product Name
MELSEC-F Series
Product Category
FX1N, FX1NC, FX3G, FX3GC,FX2N, FX2NC, FX3U, FX3UC
Series
Option, Accessories
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?