FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Starting time of the FX3U-1PG
FAQ
Starting time of the FX3U-1PG
How long does it take to actually drive the FX3U-1PG after the operation command is turned on?
Answer
It takes 1 ms or less in a unit of the motor system and 2 ms or less in a unit of the machine system.
* Motor system∙∙∙The pulse number is used as the standard for the position command.
Machine system∙∙∙μm, mdeg, and 10-4 inch are used as the standard for the position command.
* Motor system∙∙∙The pulse number is used as the standard for the position command.
Machine system∙∙∙μm, mdeg, and 10-4 inch are used as the standard for the position command.
- Product Name
- MELSEC-F Series
- Product Category
- FX3U,FX3UC
- Series
- Positioning Control