Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24944
  • Release Date : 2019/04/18 14:26
  • Print

Number of files that can be created inside a CF card in the FX3U-CF-ADP

Answer

Up to 63 files can be handled simultaneously. In addition, up to 1000 files can be created by creating FIFO function files. * The total capacity of the files must be within the CF (CompactFlashTM) capacity (specified CompactFlashTM card use ratio).
Product Name
MELSEC-F Series
Product Category
FX3U,FX3UC
Series
Main Unit, I/O Extension, Option, Accessories
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?