FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Network/Communication > Supported versions of the FX3G/FX3GC series main units for accessing the other station from CC-Link using the FX3U-16CCL-M CC-Link master block
FAQ
Supported versions of the FX3G/FX3GC series main units for accessing the other station from CC-Link using the FX3U-16CCL-M CC-Link master block
Which versions of the FX3G/FX3GC series main units support the function for accessing the other station from CC-Link using the FX3U-16CCL-M?
Answer
The main units with Ver.2.00 or later can read and write programs of the FX3 series connected to the intelligent device station and can monitor devices.
(GX Works2 with Ver. 1.87R or later is applicable.)
(GX Works2 with Ver. 1.87R or later is applicable.)
- Product Name
- MELSEC-F Series
- Product Category
- FX3G,FX3GC
- Series
- Main Unit, Network/Communication