Start main contents
Font Size
S
M
L
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Supported versions of the FX3G/FX3GC ...
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
No : 24950
Release Date : 2019/04/18 14:27
Print
Supported versions of the FX3G/FX3GC series main units for accessing the other station from CC-Link using the FX3U-16CCL-M CC-Link master block
Which versions of the FX3G/FX3GC series main units support the function for accessing the other station from CC-Link using the FX3U-16CCL-M?
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
The main units with Ver.2.00 or later can read and write programs of the FX3 series connected to the intelligent device station and can monitor devices.
(GX Works2 with Ver. 1.87R or later is applicable.)
Product Name
MELSEC-F Series
Product Category
FX3G,FX3GC
Series
Main Unit, Network/Communication
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
Number of FX3U-ENET-ADP Ethernet comm...
Input numbers of the FX programmable ...
Station number setting in the "PLC Sy...
File format that can be saved to a CF...
Connection of the FX3GC series and FX...
page top
HOME
FAQ