FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Network/Communication > Differences between the FX3UC-32MT-LT and the FX3UC-32MT-LT2
FAQ
Differences between the FX3UC-32MT-LT and the FX3UC-32MT-LT2
What are differences between the FX3UC-32MT-LT and the FX3UC-32MT-LT2?
Answer
The built-in CC-Link/LT setting differs.
For the FX3UC-32MT-LT, the built-in CC-Link/LT setting is performed with the DIP switch. For the FX3UC-32MT-LT2, the setting is performed using GX Developer.
For the FX3UC-32MT-LT, the built-in CC-Link/LT setting is performed with the DIP switch. For the FX3UC-32MT-LT2, the setting is performed using GX Developer.
- Product Name
- MELSEC-F Series
- Product Category
- FX3UC
- Series
- Main Unit, Network/Communication