FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Connection of the FX3G series and the GT1020/GT1030 series (5 V type)
FAQ
Connection of the FX3G series and the GT1020/GT1030 series (5 V type)
Is it possible to add the FX3G-422-BD to the FX3G series, and connect two GT1020/GT1030 series (5 V type) GOTs; one to the built-in port and the other to the extension port?
- Category :
Answer
Only one GT1020/GT1030 series (5 V type) can be connected to the FX3G series. To connect two GOTs, select the GT1020/GT1030 series (24 V type).
- Product Name
- MELSEC-F Series
- Product Category
- FX3G
- Series
- Main Unit