Start main contents
Font Size
S
M
L
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Connection of the FX3G series and the...
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
No : 24969
Release Date : 2019/04/23 07:19
Print
Connection of the FX3G series and the GT1020/GT1030 series (5 V type)
Is it possible to add the FX3G-422-BD to the FX3G series, and connect two GT1020/GT1030 series (5 V type) GOTs; one to the built-in port and the other to the extension port?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Main Unit
Answer
Only one GT1020/GT1030 series (5 V type) can be connected to the FX3G series. To connect two GOTs, select the GT1020/GT1030 series (24 V type).
Product Name
MELSEC-F Series
Product Category
FX3G
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
Connectors for FX3UC series
Setting for installing a memory cassette
Remote maintenance
Extension blocks and units that can b...
M8037 (forced STOP signal)
page top
HOME
FAQ