FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Positioning Control > Number of FX3U-1PG pulse output blocks that can be connected to the FX3U/FX3UC main unit
FAQ
Number of FX3U-1PG pulse output blocks that can be connected to the FX3U/FX3UC main unit
How many FX3U-1PGs can be connected to the FX3U/FX3UC main unit?
Answer
For the FX3U series, up to eight FX3U-1PGs can be connected. For the FX3UC series, up to six FX3U-1PGs can be connected.
* To connect the FX3U-1PG to the FX3UC series main unit, either of the FX3UC-1PS-5V extension power supply unit or the FX2NC-CNV-IF connector conversion adapter is required.
* To connect the FX3U-1PG to the FX3UC series main unit, either of the FX3UC-1PS-5V extension power supply unit or the FX2NC-CNV-IF connector conversion adapter is required.
- Product Name
- MELSEC-F Series
- Product Category
- FX3U,FX3UC
- Series
- Positioning Control