Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24974
  • Release Date : 2019/04/23 07:20
  • Print

Setting for installing a memory cassette

Are any settings required for installing a memory cassette to the programmable controller?
Category : 

Answer

When the programmable controller is powered on after a memory cassette is installed, the memory cassette is automatically recognized. After the memory cassette is installed, it is separated from the built-in memory of the programmable controller, and peripherals read/write data only from/to the optional memory.
Product Name
MELSEC-F Series
Product Category
FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Series
Main Unit
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?