FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Connection of a memory cassette and a display module to the FX3G series main unit
FAQ
Connection of a memory cassette and a display module to the FX3G series main unit
Is it possible to connect a memory cassette and a display module to the FX3G series main unit together?
- Category :
Answer
For the 14/24-point type FX3G series main unit, they cannot be connected together. For the 40/60-point type FX3G series main unit, they can be connected together.
* When the memory cassette and display module are used together, the program transfer function of the memory cassette is disabled. Use the display module to transfer data stored in the memory cassette.
* When the memory cassette and display module are used together, the program transfer function of the memory cassette is disabled. Use the display module to transfer data stored in the memory cassette.
- Product Name
- MELSEC-F Series
- Product Category
- FX3G
- Series
- Main Unit