FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Instruction execution complete flag
FAQ
Instruction execution complete flag
The instruction execution complete flag does not turn on.
- Category :
Answer
When a flag contact is not programmed directly under the instruction to be checked, the flag may be turned off depending on the execution status of another instruction which shares M8029. Refer to Section 6.5.2 Handling of general flags in the FX3S/FX3G/FX3GC/FX3U/FX3UC Series Programming Manual Basic & Applied Instruction Edition.
- Product Name
- MELSEC-F Series
- Product Category
- FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Series
- Main Unit