Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24990
  • Release Date : 2019/04/23 10:37
  • Print

Supported versions of the FX3U/FX3UC series main units for accessing the other station of CC-Link using the FX3U-16CCL-M CC-Link master block

Which versions of the FX3U/FX3UC series main units support the function for accessing the other station of CC-Link using the FX3U-16CCL-M?
Category : 

Answer

The main units with Ver.3.10 or later can read and write programs of the FX3 series connected to the intelligent device station and can monitor devices. (GX Works2 with Ver.1.73B or later is applicable.)
Product Name
MELSEC-F Series
Product Category
FX3U, FX3UC
Series
Main Unit, Network/Communication
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?