Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24993
  • Release Date : 2019/04/23 10:38
  • Print

Temperature input modules that can be used with FX3G series

Which temperature input modules can be used with FX3G series?
Category : 

Answer

FX3U-4AD-PT-ADP (Pt100 temperature sensor input special adapter), FX3U-4AD-PTW-ADP (Pt100 temperature sensor input special adapter), and FX3U-4AD-TC-ADP (K/J type thermocouple thermometer input special adapter) are available.
Product Name
MELSEC-F Series
Product Category
FX3G
Series
Analog Control
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?