Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24998
  • Release Date : 2019/04/23 10:38
  • Print

Remote maintenance

How can I change programs used in a remote facility?
Category : 

Answer

Remote maintenance can be performed by writing a program to a memory cassette and sending the program or by using a personal computer (GX Developer). With a programmable controller that supports the memory cassette equipped with the loader function, data in the memory cassette can be easily written to the built-in memory of the programmable controller without a personal computer (GX Developer) at the destination.
Product Name
MELSEC-F Series
Product Category
FX1S, FX1N, FX1NC, FX3G, FX3GC,FX2N, FX2NC, FX3U, FX3UC
Series
Main Unit
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?