FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27 > Enabling the object gesture function
FAQ
Enabling the object gesture function
How can I enable the object gesture function?
Answer
The object gesture function can be enabled when the following conditions 1. and 2. are both satisfied.
◆ GT Designer3 (GOT2000) Version 1.100E or later
1. Enable the gesture function in the project setting.
Select [Common] - [GOT Type Setting], and then select [Use the gesture function].
2. Turn off b0 of the Gesture Common Control (GS1794).
Set the following item as well to enable the object gesture function in the video/RGB display object.
◆ GT Designer3 (GOT2000) Version 1.130L or later
Select [Object], and the [Video/RGB Display] dialog appears. Select [Gesture Operation (Scaling/Scrolling)] for [Touch Mode] on the [Video/RGB Setting] tab.
◆ GT Designer3 (GOT2000) Version 1.100E or later
1. Enable the gesture function in the project setting.
Select [Common] - [GOT Type Setting], and then select [Use the gesture function].
2. Turn off b0 of the Gesture Common Control (GS1794).
Set the following item as well to enable the object gesture function in the video/RGB display object.
◆ GT Designer3 (GOT2000) Version 1.130L or later
Select [Object], and the [Video/RGB Display] dialog appears. Select [Gesture Operation (Scaling/Scrolling)] for [Touch Mode] on the [Video/RGB Setting] tab.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture)
- Series
- GOT2000 Series
May I have your opinion?
Related FAQ
- Gesture functions available for the alarm display
- Disabling the object gesture function
- Object gesture function while using the GOT remote access function
- Touch Status External Notification (coordinate) during the screen gesture mode
- Screen gesture function when the video/RGB input screen is displayed