FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27 > Screen gesture function while using the GOT remote access function
FAQ
Screen gesture function while using the GOT remote access function
Can I use the screen gesture function from the VNC client while using the GOT remote access function (VNC server function)?
Answer
You cannot use the screen gesture function from the VNC client while using the GOT remote access function (VNC server function).
If the VCN client obtains the authorization while the GOT is in the screen gesture mode or displays the screen enlarged with a pinch-out operation, the GOT cancels the screen gesture mode or enlarged screen, and displays the normal-sized screen (100%).
The VNC client also displays the normal-sized screen (100%).
After the authorization is transferred to the GOT, switching to the screen gesture mode is enabled on the GOT.
If the VCN client obtains the authorization while the GOT is in the screen gesture mode or displays the screen enlarged with a pinch-out operation, the GOT cancels the screen gesture mode or enlarged screen, and displays the normal-sized screen (100%).
The VNC client also displays the normal-sized screen (100%).
After the authorization is transferred to the GOT, switching to the screen gesture mode is enabled on the GOT.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), GOT function (VNC server)
- Series
- GOT2000 Series