FAQ


FAQAbout Products
 
 - FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Displaying overlap windows in screen gesture mode
FAQ
Displaying overlap windows in screen gesture mode
Can overlap windows be displayed in screen gesture mode?
- Category :
- 
      - FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
 
Answer
Overlap windows cannot be displayed in screen gesture mode. 
If a request to display the overlap window is received in the screen gesture mode, the overlap window is displayed after screen gesture mode is disabled.
* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), GOT function (standard function)
- Series
- GOT2000 Series, GOT3000 Series