Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23522
  • Release Date : 2018/09/14 15:07
  • Print

Using the rugged model outdoors

Answer

The rugged model can be used outdoors.
Protect the GOT from direct sunlight by attaching a roof or in other ways when using the rugged model outdoors.
Due to direct sunlight, the temperature of the panel surface and inside the control panel may increase. Use the GOT in the environment within the operating ambient temperature range.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Rugged model
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?