Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • No : 23607
  • Release Date : 2018/09/14 15:09
  • Print

Alarm E7

Answer

Alarm E7 (Controller forced stop warning) occurs when an forced stop is executed by the Positioning module or the Simple Motion module.
The following shows how to cancel the alarm.
(1) When not using the forced stop input signal
    Set "[Pr.82] Forced stop valid/invalid selection" to "Invalid."
(2) When using the forced stop signal
    Supply 24 VDC power for the forced stop input signal.
Product Name
Simple Motion module/
Positioning module
Series
MELSEC iQ-R
MELSEC iQ-F
MELSEC-Q
MELSEC-L

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries