Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23611
  • Release Date : 2018/09/14 15:09
  • Print

BUSY signal

Answer

No. The motors' operation is not completely linked to ON/OFF timing of the BUSY signals.
BUSY signal is turned ON when the controller starts sending commands to the axes, and turned OFF when the command sending is complete.
However, servo motors continue to drive until the deviation counter becomes "0".
Product Name
Simple Motion module/
Positioning module
Series
MELSEC iQ-R
MELSEC iQ-F
MELSEC-Q
MELSEC-L
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?