Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23612
  • Release Date : 2018/09/14 15:09
  • Print

BUSY signal

Answer

The BUSY signal turns ON even when position control of movement amount "0" is executed.
However, since the ON time is short, the ON status may not be detected in the sequence program.
Product Name
Simple Motion module/
Positioning module
Series
MELSEC iQ-R
MELSEC iQ-F
MELSEC-Q
MELSEC-L

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries