Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23612
  • Release Date : 2018/09/14 15:09
  • Print

BUSY signal

Answer

The BUSY signal turns ON even when position control of movement amount "0" is executed.
However, since the ON time is short, the ON status may not be detected in the sequence program.
Product Name
Simple Motion module/
Positioning module
Series
MELSEC iQ-R
MELSEC iQ-F
MELSEC-Q
MELSEC-L
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?