Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20830
  • Release Date : 2018/08/22 16:24
  • Print

Seamless communication of FR Configurator SW3

The master and remote I/O station of the programmable controller is connected via the MELSECNET and the inverter is connected to the CC-Link unit of remote I/O. With this configuration, is the CC-Link Seamless communication available?
Category : 

Answer

The communication via the MELSECNET is not available.
Product Name
Inverter, magnet motor drive
Product Category
Engineering software
Series
FR Configurator SW3
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?