FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > Built-in PLC function
FAQ
Built-in PLC function
What causes the error: 2200 (MISSING PARA) in the PLC function?
- Category :
Answer
The error indicates that the parameter setting of the PLC function is not set. It is considered that the PC parameter is not checked when the PC parameter and program are written to the PC.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800