Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20889
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800-R2R

When the winding diameter calculation is performed in the thickness method by using the motor with encoder, can I use only winding diameter compensation under the normal speed control?
Category : 

Answer

It is possible when the dancer control and tension sensor feedback speed control is used and the PID calculation is turned OFF. Because the PID compensation cannot be used and no compensation is performed for disturbance, the accuracy decreases.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800-R2R

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries