Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20914
  • Release Date : 2018/08/22 16:25
  • Print

Monitoring function of the FR-A800-R2R

Can I monitor Pr.52 = 26: Line speed command, 27: Actual line speed, and 31: Line speed pulse monitor while the operation is stopping? Is there any requirement for the monitor indicator?
Category : 

Answer

Line speed command and Line speed pulse monitor can be monitored while the operation is stopping. Actual line speed monitor becomes "0" while the operation is stopping. Line speed pulse monitor can be monitored while the operation is stopping only when Pr.362 = 1, 2, or 7. When Pr.361 = 1, 2, or 7 and Pr.362 = 1, 2, or 7, the input of Pr.361 is disabled as the functions are duplicated.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800 Plus

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries