FAQ


FAQAbout Products
 - FAQ > Drive Products > Inverters-FREQROL > FR-A800
 
FAQ
FR-A800
      Though the control circuit temperature can be monitored with Pr.52=98, is any alarm generated when the control circuit temperature rises?
    
  - Category :
 
Answer
    No alarm occurs due to the abnormal temperature. In the main circuit, alarms such as heatsink overheat will be occurred.
  
    - Product Name
 - Inverter, magnet motor drive
 
- Product Category
 - Inverter
 
- Series
 - FR-A800