FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Options > FR-A842
FAQ
FR-A842
Is the inrush current limit circuit built in the FR-A842? If it is not built in, is there any problem combining it with the FR-HC2?
- Category :
Answer
The inrush current limit circuit is not built in the FR-A842 (inverter unit). It is built in the FR-CC2 (converter unit), which is combined with the FR-A842. There is an inrush current limit circuit in the outside box of the FR-HC2. Thus, there is no problem for combining the FR-A842 with the FR-HC2. When the FR-HC2 is used, the FR-CC2 is not required.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800