Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21147
  • Release Date : 2018/08/22 16:26
  • Print

FR-HC2

What is the cable gauge of the inrush current limit resistor (FR-HCR2) of the FR-HC2?
Category : 

Answer

It is 0.88 mm2 (AWG18), and 0.3 mm2 (AWG24) for the thermostat.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries