FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > 400 V inverter
FAQ
400 V inverter
Does the 400 V inverter run with 400 V input to the main power supply and 200 V input to the control circuit power supply?
- Category :
Answer
No, it does not run. "Err" is displayed when it is operated. Always input the same voltage (400 V) to the main power supply and control power supply.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-F700P, FR-F700